AXIS#.SAFEPARAM.SLI_#.FSOE

Description

Indicates if the Safely Limited Increment (SLI) safety function can be activated through FSoE. This parameter can only set to “Used” when FSoE is activated (SAFEPARAM.SAFEFIELDBUS.ACTIVATION is set to 1 – “Activated”).

Value

Description

0

Not used

1

Used

 

Parameters Editor with FSoE options displayed and circled

Context

For complete SLI information refer to SLI (Safely Limited Increment).

Related safety parameters:

Versions

Action Version Notes

Implemented

02-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Not used)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLI_1.FSOE

3169h

03h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLI_2.FSOE

316ah

03h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLI_3.FSOE

316bh

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_1.FSOE

3269h

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_2.FSOE

326ah

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLI_3.FSOE

326bh

03h

Unsigned8

-

-

Read/Write

No